What are the maximum groups of variables, maximum offset groups of workpiece coordinates, and maximum tool length compensation groups that the Delta's CNC controller can provide?What are the maximum groups of variables, maximum offset groups of workpiece coordinates, and maximum tool length compensation groups that the Delta's CNC controller can provide?
A:The Delta’s CNC controller can support up to 700 groups of variables. The available variables are numbered from #1601 to #1800 and from #10001 to #10500. Delta’s CNC controller can also provide a maximum of 70 offset groups of workpiece coordinates and a maximum of 100 groups of tool length compensation.