Why is it necessary to improve the power factor of a factory plant? What are the benefits?A low power factor could result in energy loss and increase all types of operation costs. Delta’s APF2000 series can improve the power factor to 1 and provide the following benefits :
‧Increase the load carrying capability of the power system
‧Improve voltage capacity of equipment
‧Reduce power system loss
‧Reduce energy loss in a transformer
‧Avoid penalties from a utility company due to low power factor