A user must estimate how much power quality distortion needs to be modified and select one or multiple APF2000 units. The APF2000 series provides various models with different ampere ranges for users to match with their system needs. It supports parallel connection of up to 6 units for larger system requirements. Please refer to the wiring diagram below for installing one or multiple APF2000 units.
Figure 1 - One APF2000 unit installation

Figure 2 - Multiple APF2000 units installation