Yes. The APF2000 provides the EREMOTE function for users to monitor and control the APF2000 installed at the factory site. Simply follow the steps below for setting up a remote control function.
Figure 1 - Set IP and Gateway using the HMI screen on the APF.

Figure 2 - Install EREMOTE to the computer and input the APF2000 IP address.