FAQ

The biggest difference between the APF2000 Series and the SVG2000 Series is that the APF2000 Series can filter out 2~50th order harmonics, while the SVG2000 Series can only filter out up to 13th order harmonics. Regarding compensation capability, the APF300A model of APF2000 Series can provide compensation to a maximum 300A current. However, the compensation provided by the SVG-500A63A model of the SVG2000 Series can reach up to a maximum 720A current. Thus, the APF2000 Series is suitable for applications which require high order harmonics suppression and power factor improvement. The SVG2000 Series is suitable for applications where there is harmonic current or a surge current that occurs at impact load.
‧AFE2000: Active Front End
Delta's AFE2000 Series is a controllable rectifier that uses PWM modulation to greatly reduce distinct peaks of current and form perfect sine wave current. Using the AFE2000 Series the power factor is corrected and high order harmonics are eliminated. In addition, the AFE2000 Series can replace traditional brake resistors, convert the regenerative energy into reusable electricity, and send it back to the mains to reduce total energy consumption. The AFE2000 Series is connected in serial to the grid and the loads, which differs from the APF2000 Series and SVG Series. The AFE2000 Series is suitable for applications, which need to measure the power quality for individual control and compensation.
-Individual control: Install before an individual device for treatment of a large load device.