How many detection windows does Delta’s DMV Series machine vision system support for each project?Each project supports 128 (W000~W127) detection windows. As the windows are processed in ascending order, positioning functions should be set to a smaller ID so that the position can be referenced later by the system. Please reserve the first few IDs for detection window positioning functions. It is recommended that you edit the detection window starting from ID W005.