What are the sizes of pressure connections that Delta pressure sensors support?Delta pressures sensors support 3 types of connections. For the P type, the outer connection is PT 1/8 and the inner connection is M5. For the N type, the outer connection is NPT 1/8 and the inner connection is M5. For the G type, the outer connection is G 1/8 and the inner connection is M5.