IFD8520 functions as 1) "addressable" communication converter and 2) communication module. When used as communication modules, it only supports ASCII, not including RTU, and the data conversion direction is RS-485/422-->RS-232. Below is the screen showing successful IFD8520 gateway connection.