Why is temperature still unstable with PID control?Considering the system demand, PID control provides the controller with three parameters, P (Proportional Band), I (Integral Time), D (Derivative Time) and PID is automatically set when AT (Auto Tuning) is active. By activating AT function, the parameters will be generated automatically to reach a more accurate execution. Also, the parameters can be set and adjust by manual setup.