What is CT (Current Transformer) function used for?When controller performs outputs, system will be activated by the current in circuit. By using CT function, it is possible to check if the current value is within allowable range. If current value is lower or higher than the set value, CT function can be used with alarm output function to warn the users when the current exceeds the set value.