What is PID programmable (Ramp Sock) control used for?The PID control is to maintain the output at a level so that there’s no error between the process value and the set value. User can use PID programmable control to set the parameters for the set value by time sequence in order to switch different user-defined set value so that the temperate can be maintained or rise very efficiently and quickly to achieve sequence control.