Only DTE series temperature controllers (V1.5 and later versions) have the "slope control" function.
● Example:
Assume PV = 20°C, SV = 100°C, slope = 10.0°C/min.
Thus, (100 – 20)/10.0 = 8 (this means it takes 8 minutes to heat up to the target temperature)
● How do you write 0020 to the 4824H register?
Assume the address is set to "1", send the command "010647F112347B CR LF" to enable the write-to-flag function. Next, send the command "0106482400206D CR LF" to enable the flag for slope control.
● How do you set up the slope? (Unit: 0.1°C/min.)
Ex: Set the slope for CH1 to 10.0°C/min. The communication addresses for slopes will be:

Send the command "0106197000640C CR LF" to write 10.0°C /min. as the slope for CH1.