How many lines can be edited at most in one macro command? If not enough, how to solve this problem?Up to 512 lines can be edited in one macro command. If not enough, the users can write some functions in sub-macro command. The maximum lines that could be edited in one sub-macro command are 512 lines as well.