Is it possible that the function of SYS system key becomes disabled and not provided for the users to use it? Yes, it is possible. The users only need to set the “System Key Use Mode” option to “Disable” located in the Configuration dialog box under the Default tab.