If the users forget the password and the programs can not be used, what should they do?Concerning the intellectual property rights, we do not provide the service for decoding. So the users must remember their passwords, or they will not be able to upload or compile. If they are unable to enter into system screen, they can solve this problem by downloading a screen without password protection.