Sometimes the communication speed seems to be a little slow when DOP series HMI uses non-consecutive PLC addresses to conduct the communication. How can I accelerate the communication speed?Both Screen Editor 1.05.82 and later version (for DOP-A series) and Screen Editor 2.00.15 and later version (for DOP-B series) support Delta DVP Q-Link controller. Connecting to this controller makes it possible to read all non-consecutive PLC addresses at a time and deliver the command so as to enhance the communication speed efficiently.