When the baud rate is higher, if the data transmission speed is faster as well?This is not exactly true. Sometimes, when the baud rate is over high, the controller may not be able to response in real time. When the controller cannot response in real time, it may result in communication retry and slow the communication down.