What is the benefit of the recipe function?The benefit of the recipe function is that the users do not need to change a lot of parameters manually. When manufacturing more than one product, the recipe function can help to change all of the parameters just one time.