How can a CAM chart be created on the DVP20PM?There are two ways to create a CAM chart.
1. Draw E-CAM curves from the CAM chart.
2. Generate E-CAM data from DTO instructions.
The CAM chart draws the curves from point-to-point or via functions.
The DTO instructions automatically create flying shear curves. Users can set relevant parameters and operation requirements for the actual structure of the flying shear. E-CAM curves that meet these requirements can then be created and utilized.