What are the resolution and range of analog output and digital data for the Delta Slim Type analog output module, respectively? There are 12 bits of resolution for the analog output module DVP02DA/DVP04DA, a range of 0 ~ 10V for the analog voltage output, and a range of 0 ~20mA for the analog current output. All correspond to the range of 0 to 4,000 for digital data.