What are the resolution and range of analog output and digital conversion for the Delta Slim Type analog input module, respectively? The range of analog input voltage for the analog input module DVP04AD/DVP06AD is ± 10V while the range of digital conversion and resolution are ± 8,000 and 14 bits. The range of analog input current is ± 20mA while the range of digital conversion and resolution are ± 4,000 and 13 bits.