Delta Ethernet module DVPEN01-SL transmits data through which communication protocol? Any other functions for users’ applications?DVPEN01-SL transmits data through the standard Modbus TCP. Other functions include:
(1)Email: Set up a recipient email address to send the content of the PLC registers.
(2)Data exchange: 2 DVPEN01-SL modules with DVP-SV series PLCs connected are able to synchronously read or write 100 words of data.
(3)RTU function: With Delta Ethernet remote I/O module RTU-EN01, the DVPEN01-SL is able to achieve mapping functions, monitoring remote AI/AO and DI/DO.
(4)IP filter: You can restrict misconnections, preventing the parameters set in the DVPEN01-SL from being modified by the misconnections.
(5)Password protection: Set the DVPEN01-SL’s IP address, email recipient, data exchange area, RTU and IP filter functions and lock them with a password.