FAQ

Notes:
1.The simulator is only for testing programs when the user does not have a PLC. The result of the simulation will not be exactly the same as that from a PLC execution. You still have to test the program on an actual PLC before running the program.
2.The simulator does not support the following instructions: WDT, REF, REFF, MTR, DHSCS, DHSCR, DHSZ, SPD, PLSY, PWM, PLSR, IST, TKY, HKY, DSW, SEGL, ARWS, ASC, FROM, TO, RS, PRUN, VRRD, VRSC, ABS, PID, MODRD, MODWR, FWD, REV, STOP, RDST, RSTEF, SWRD, DELAY, GPWM, FTC, CVM, MEMR, MEMW, MODRW, PWD, RTMU, RTMD, RAND, DABSR, ZRN, PLSV, DRVI, DRVA, DPPMR, DPPMA, DCIMR, DCIMA, DPTPO, HST, DCLLM
3.The simulator in WPLSoft supports error detection. For details, see chapter 12 in "Help" for WPLSoft.