What should I pay attention to when using the Z phase signal for the Z axis of the DVP20PM00M (Delta’s professional motion controller)?1.For the DVP20PM00M, the zero point signal input for the Z axis is X3. It is an open collector contact input on the internal circuits of the PLC used for the OCZ signal of the connected AC servo drive.
2.The generation of a Z phase signal can be verified by the D1805 input terminal when conducting program monitoring.
3.Please observe the following wiring notes when wiring:
a.Ensure that SS2 on the PLC is connected to a +24V power supply.
b.Ensure that 24G on the PLC is connected to the ground terminal on the servo drive.
c.Ensure that X3 on the PLC is connected to the OCZ terminal on the servo drive.