Delta's AH500 Series supports international standard MODBUS protocols and connections which can be established with the RS-232, RS-422 and RS-485 communication interfaces. Enable ISPSoft software, follow the steps below and users can define the desired serial communication type easily.
STEP 1: Double click HWCONFIG

STEP 2: Double click CPU

STEP 3: Select COM Port item and type