On the output terminal block of DVP-ES2/EX2 transistor output type PLC MPU, there are two different terminals, UP and ZP. How can I wire these two terminals? What are their functions?All transistor outputs of DVP-ES2/EX2 series PLC contain diode for back EMF protection, which is sufficient for small-power conductive load and average ON/OFF application frequency. However, in big-power or high ON/OFF frequency environments, please connect to another suppression circuit (as shown in the figure below) to lower the noise and prevent damages on the transistor output circuit resulting from over-voltage or overheating.
The transistor outputs are all open collector; therefore, if Y0/Y1 is set to be pulse output and to ensure the transistor module works normally, the pull-up resistor has to be maintained at output current > 0.1A.
Circuit wiring for transistor output: