What are the differences between EH2 and EH, and can they compatible the same extension module?EH2 do a lot changes on hardware design, it improve the communication performance between MPU and extension module and need only 1ms. Because the hardware design is different, the module is different, too.