What is the limitation of the bandwidth of SC?The bandwidth of SC pulse output+ counter is 130KHz, and in firmware V1.2 and V1.4 support two axis output pulse at the same time. Y10 is 60k max, and Y11 has to be lower than Y10 and 40k max. So the bandwidth of counters is only 30k, but high speed counter X10 and X11 are not limit by it. High speed counter can reach 100k max and 130k totally.