How to decide Kp、Ki、Kd of PID instruction?When first executing PID, suggest to set auto-tuning mode. And the sampling time depends on the environment. If the value changes rapidly then the sampling time has to be set smaller.
After auto-tuning, check the temperature curve, if raising rapidly, suggest to reduce Kp, if shaking too strong, suggest to reduce Ki. Please refer the user manual for more information.