Do Delta PLC provide online editing function?WPLSoft 2.09 provides online editing function, can download program while PLC is running.
The limitation of SA_V1.4/SX_V1.4/SC_V1.2/EH2/SV is 49 STEPS, other firmware version SA/SX/SC/EH/EH2/SV is 15 STEPS。