How can I identify the axis type of the LPR Linear Pocket Actuator?The LPR Linear Pocket Actuator is available in two axis types: rotary and linear. Check parameter PM.000 to determine the axis type: PM.000 = 0 indicates a rotary axis, while PM.000 = 2 indicates a linear axis.