How do I verify whether the CT on APF3000 is installed in the correct orientation?Set parameter 06-08 to 1 and wait for 06-09 to display the result. A value of 2 indicates correct wiring, 3 indicates incorrect writing, and 4 indicates the load current is too low.