When a high-power motor drive is used to operate a low-power motor, excessive current may occur under certain operating conditions, potentially causing motor overheating and damages. It is therefore recommended to configure protection parameters that allow users to define appropriate thresholds. If the current exceeds the specified limit, the motor drive will trigger an alarm or fault notification, providing timely warnings and helping prevent motor failures.
This function can be implemented by configuring over-torque protection parameters, as shown in the steps below: