First, set the trigger method to “Program Control”. Then, use SM700 - SM827 (Enable flags for Modbus TCP data exchange connections 1 - 128) to activate required data exchange connections. Use SM828 - SM955 (Error flags for Modbus TCP data exchange connections 1 - 128) to check for data exchange anomalies, such as the slave response error code.