The FW version after 1.0.7.2 will support the FTPS function on AX-8 Linux series motion controller, which will be released in Q4 2025.
Please go to the controller’s
System Parameters page, set the FTP mode to FTPS, and enable the FTP server.
After downloading the project into the AX-8, please power cycle the AX-8 to make the settings valid. Afterwards, you may use third-party software to test the FTPS function, such as FileZilla.