Which Delta PLC Series supports EtherCAT motion control?Delta’s AS300 and AX Series both support EtherCAT motion control. The AS300 Series requires the AS-FECAT function card to enable EtherCAT communication and supports single-axis motion control only. The AX Series features built-in EtherCAT communication and supports multi-axis synchronous motion control.