When installing DIAScreen, the system automatically installs the eRecordViewer software. Open eRecordViewer and import the CSV file you want to check. If the checksum verification is successful, a green bar will appear along with the message “Verified passed.”

If the verification fails, a red bar will be displayed and the number of failed items will be listed, as shown in the figure below.