Please refer to the tables below to find the proper setting for your application.
| Baud Rate (bps) |
Max. Length (m) |
Max. Stations |
| 1200 ~ 19200 |
1200 |
32 |
| 38400 |
1200 |
24 |
| 57600 |
1200 |
16 |
| 57600 |
1200 |
18 |
| Baud Rate (bps) |
Max. Length (m) |
Max. Stations |
| 1200 ~ 19200 |
1200 |
32 |
| 38400 |
900 |
32 |
| 57600 |
600 |
32 |
| 115200 |
300 |
32 |
We also have the RS485 repeater IFD8510-A, which can extend the communication length. You can find it on our website
Delta | Download Center (deltaww.com).