Is it possible to install a DVP or AS PLC in a vertical orientation?Yes, it is possible to install DVP or AS PLCs in a vertical orientation, but it may affect the heat dissipation. As a conservative estimate, the operating temperature may be reduced by an additional 10 degrees Celsius.