Step 1: Log in with the details (Username: user ; Password: 2222).
Image 1
Step 2: Click on “Platform Settings” and enter the device connection page
Image 2
Step 3: Select “Scan” to connect to the camera. Then, click the gear icon to enter the parameter editing page.
Image 3
Step 4: Click the drop-down menu and change authority to “Guru” and start editing all camera parameters.
Image 4