FAQ
How do I use the multi-speed function? (Take the Delta Vector Control Drive C2000 as an example)Use the multi-function input terminals to configure Command MI1~MI4 (Pr.02-01~02-04), and configure multi-step speed (frequency) with Pr.04-00 to Pr.04-14 as shown in the following diagram.
The chart below shows the multi-step speed configuration and external terminals sequence in combination with the change of speeds.

Have a question? We'd love to hear from you. Inquiry