You can check the status value on the TCP/IP connection tab under the Tag page. The value 0 means there is no error and the connection is normal. For any other value, you can use the F1 shortcut key and enter "TCP/IP Port Tags" to look up the meaning of the error code.