Step 1: Go to Delta’s
Download Center → Download
DRAStudio V1.00.XX.XX → Install DRAStudio. Please make sure the folder path is correct.
Step 2: Open the default path C:\Delta Industrial Automation\DELTA_IA-Robot_DRAStudio-V1-00-XX-XX, or refer to the path of previous installations → Open API file → Industrial Robot offers three API types (C++ / C# / Labview)
Step 3: Unzip “DROE_API_CS.zip” → Refer to “NewAPI Application Manual_20231017_V3.pdf”. Open “DROE_CSharp_API_Sample.sln” file with Visual Studio and start developing.