In JOG, MPG (hand wheel), Homing and Manual modes, please refer to the following steps to set the rotation speed of the spindle axis (spindle speed) directly:
‧Press the PRG key to switch to the program and coordinates combine screen as illustrated below
‧Press the F1 key and the S set dialog box pops up
‧Enter the desired spindle speed (S command) and press the Enter key to complete the setting