You can set the function by configuring parameters. As shown in the image below, the relevant parameters include Pr. 00-20 (master frequency command source), Pr. 00-35 (auxiliary frequency command source), and Pr. 00-36 (master/auxiliary frequency selection). Please consult Chapters 11 and 12 of the MS300 User Manual for parameter descriptions, and set the parameters based on your specific needs.
Image: Master and auxiliary frequency parameters