The full-closed loop control of Delta's CNC Solution utilizes Delta's servo drives which feedback signals from the main encoders and linear scales for real-time compensation. The linear scale can be connected to a servo drive. The high frequency response of Delta's servo drive offers the system better compensation with higher precision than if commands are made by the CNC controller itself.