What are the features of Delta’s CNC Solution for applications such as high-speed drilling and tapping?1.For M6X1 tapped holes, the tapping speed of Delta’s CNC Solution can reach 6000 rpm. This is the highest speed for medium-level CNC machine tool systems in the world.
2.When connected with Delta’s C-Box power storage, Delta’s CNC Solution can save over 70% more energy than when using brake resistors for continuous tapping.