Yes. The connector wiring of the CNC B Series’ second operating panel is compatible with CNC A Series. Users only need to adjust the MLC programming setting based on the differences of the panel keys’ X input signals.
For the appearance and key signal definitions of the B Series’ second operating panel, please refer to Chapter 3, "Wiring", in the product’s operation and maintenance manual.