What kinds of functions does the ASD-DMC-RM04PI pulse output module support? (ASD-DMC-RM04PI is an extension module for the connection of Delta’s PCI-DMC-A01 DMCNET motion control card) 1.200KHz pulse outputs for 4 axes (supports Pulse + Direction, Clockwise (CW) + Counterclockwise (CCW) pulse and AB phase pulse)
2.200KHz pulse inputs for 4 channels (supports Clockwise (CW) + Counterclockwise (CCW) pulse and AB phase pulse)
3.Built-in 8 digital inputs and 8 digital outputs (2 digital inputs and 2 digital outputs for each axis).
4.Each axis has forward limit, reverse limit and zero point.
5.There are two kinds of control modes for selection:
(1) When the four axes share the same station number, the interpolation can be used for the same module only.
(2) When each axis occupies one station number, different modules can use interpolation to work with other servo axes.