Step 1: Select the image file you would like to change. The image format should be *.bmp, *.jpg or *.png.
Step 2: Take the *.png image file for example: Users should name the startup image as SplashScreen.png, and the icon as ICON.png.
Step 3: Place the image files in the following DMV-VGR default installation path for the software.
C:\Program Files (x86)\Delta Industrial Automation\DIAVision\DMV-VGR
Step 4: Open the DMV-VGR software, the startup image and icon are changed to the selected image files.
Image 1. Software startup image
Image 2. Icon